Classic Modules

E - Communication with SIMATIC S7

 

E1 - Ethernet communication with CP343-1 IT

In this module, the reader learns how an ISO connection is commissioned on the Ethernet between two S7-300s with the CPU-342-1 IT communication processor.

Training curriculum (PDF)

DE


E2 - Web technologies of the CP343-1 IT

In this module, the reader is acquainted with the application options and use of web technologies in automation systems. The necessary steps for this are represented on the basis of a "CP343-1 IT" module. As an example, the visualization of a tank is used, in which the current process values can not only be displayed, but also modified. In addition, the specified tank applet is extended with further functions in order to obtain an insight into the development of user-defined applets.

Training curriculum (PDF)

DE


E3 - Internet connection for CP343-1 IT

In this module, the reader is acquainted with the options and techniques for connecting programmable logic controllers to the Internet. The necessary steps for this are represented using the example of a "CP343-1 IT" module and a Bintec ISDN router.

Training curriculum (PDF)

DE


E4 - PROFINET with IO controller CPU 315F-2 PN/DP and IO device ET 200S

In this module, the reader learns how PROFINET is commissioned with the CPU 315F-2 PN/DP as IO controller and the ET 200S as IO device.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

S7 project (ZIP)

DE

EN


E5 - PROFINET with IO controller CPU 343-1 Advanced and IO device ET 200S

In this module, the reader learns how PROFINET is commissioned with the CP343-1 Advanced as IO controller and the ET 200S as IO device.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

S7 project (ZIP)

DE

EN


E6 - PROFINET/PROFIBUS DP with CPU 315F-2 PN/DP, IE/PB Link and DP slave ET 200S

In this module, the reader learns how PROFIBUS DP components can be integrated with PROFINET. It shows how the CPU 315F-2 PN/DP is commissioned with the IE/PB link as network transition and an ET200S as DP slave.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

S7 project (ZIP)

DE

EN


E7 - Diagnostics on the PROFINET with CPU 315F-2 PN/DP IO controller / SCALANCE X208 switch and ET 200S IO device

In this module, the reader learns how diagnostics can be performed objectively on the PROFINET. This uses a configuration with a CPU 315F-2 PN/DP as IO controller, the ET 200S as IO device and a diagnostics-capable SCALANCE X208 switch.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

S7 project (ZIP)

DE

EN


E8 - PROFIsafe and PROFINET with IO-Controller CPU315-2 PN/DP and IO-Device ET200s

The reader learns how a safety-related application is started up on the PROFINET (PROFIsafe).

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

S7 project (ZIP)

DE

EN


E9 - PROFINET with 2x CPU 315F-2 PN/DP

In Module E09, the reader learns how two PLCs with the CPU 315F-2 PN/DP can communicate with each other via PROFINET. Module E09 shows the method for startup in principle, using a brief example.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

S7 project (ZIP)

DE

EN


E10 - Component Based Automation (CBA) with 2x CPU 315F-2 PN/DP and iMAP

The reader learns networked how two stations can be generated as CBA components, in order to be networked with IMap into an overall project. The two stations CPU 315F-2 PN/DP are used as PLCs. They are interconnected by means of PROFINET. Module E10 shows the method in principle, using a brief example.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

Projects (ZIP)

DE

EN


E11 - Radio Frequency Identification (RFID) with SIMATIC S7-300F-2PN/DP and RF180C

In this module, the reader learns how to commission networting and data exchange between PLCs and RFID-components.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

Instructions (ZIP)

DE

EN

Templates (ZIP)

DE

EN

S7 project (ZIP)

DE

EN


E12 - Vision Sensor Shape Checking with SIMATIC S7-300F-2PN/DP and VS120

In this module, the reader learns how to commission networting and data exchange between PLCS and the Vision Sensor VS120.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

Instructions (ZIP)

DE

EN

Templates (ZIP)

DE

EN

S7 project (ZIP)

DE

EN


E13 - Vision Sensor Reading Code with SIMATIC S7-300F-2PN/DP and VS130-2

In this module, the reader learns how to commission networting and data exchange between PLCS and the Vision Sensor VS130-2.

Training curriculum (WORD)

DE

EN

Training curriculum (PDF)

DE

EN

Instructions (ZIP)

DE

EN

Templates (ZIP)

DE

EN

Software (ZIP)

DE

EN

S7 project (ZIP)

DE

EN