Monitoring and controlling the biogas plant

A biogas plant has to be monitored and controlled. As well as accounting for all the quantities of materials brought in and produced, it is particularly important to fulfill the documentation duties for the gas and energy production. A certain degree of automation ensures profitable and trouble-free operation of the plant.

The measurement and automation concept required depends on the size and type of the plant, and the specific requirements. For example, the operator station or control room can be located in the estate or technical building. It is, of course, also possible to operate and maintain a plant by remote access, with alarms issued by SMS.