SIMATIC STEP 7 Basic V11

Engineering Software for applications with the SIMATIC S7-1200 controllers

Description

SIMATIC STEP 7 Basic V11 is a budget-priced subset of the STEP 7 Professional controller software in the TIA Portal, which is used for the engineering of SIMATIC S7-1200 micro controllers and for configuring SIMATIC HMI Basic Panels, as WinCC Basic is part of the software package.

Due to its integration in the engineering framework of the TIA Portal SIMATIC STEP 7 Basic offers the same advantages as the STEP 7 Professional engineering software e.g. direct on-line diagnosis, simply adding of technology objects or the library concept for time-saving and efficient reusing of data.

STEP 7 Basic V11 offers the IEC programming languages LAD (Ladder Logic) as well as FBD (Function Block Diagram).

For more information on STEP 7 Basic V11 see the webpages about STEP 7 Professional V11 and the TIA Portal Engineering Framework.