Customer benefit

The City of Oslo is Convinced

After already 83 three-part metro trains were commissioned into operation on the rail network of 85 kilometers, the city of Oslo ordered in 2010 additional 32 trains.

  • 30 % less energy consumption in comparison to the predecessor model

  • an operating train filled to capacity has a CO2 emission rate of only 0.3 g per passenger

  • The recycling rate of 95 % reduces the emission by an additional 405 tons per train due to the saving in primary resources

  • Reduction of environmental impact up to 20 %


Excellent conceptional framework: Amongst others, the Metro Oslo from Siemens was honored with the "Sustainable Product Award" of the Technical University in Vienna, the EEP Award, and the Createch Award.