Tools

Siemens Global WebsiteSiemens Global Website

Download complete Image of International Editions

General information about full version download

Hardware and software requirements

  • PC with 2 GHz CPU or faster

  • 2 GB RAM

  • Windows 7 / Windows 8.1 / Windows 10

  • Screen resolution 1024 x 768 pixels or higher (1280 x 1024 recommended)

  • 13.0 GB of free hard disk memory (temporary)

  • 8.5 GB of free hard disk memory (complete installation)

  • 2.0 GB of free hard disk memory for each further data package (optional)


Further Information

For further information please see the document below

DVD Inlay International Edition (English)

Download International Editions (04/2017)

Please refer to the release notes for more version details.

Installation instructions

  • unzip the downloaded zip archive to an empty folder

  • run Setup.exe in the main folder of the unzipped archive

  • please be aware that the complete contents of the archive has to be unzipped first, executing Setup.exe directly form within the archive will fail!


Determine your current software version by selecting the 'Help' menu from inside the program and selecting 'About'.

Alternatively the unpacked image archive can be burned on a DVD or copied on a USB stick.

Problems during the CA 01 download

If any problems should occur during the download process, please note the possibility to order a DVD either via your Siemens sales contact partner or using the link below:

Ordering CA 01 DVD