Tools

Siemens Global WebsiteSiemens Global Website

LanguageLanguage
Close language layer

Switch language to:

The Siemens Industry Automation Division has expanded its Simatic Ident portfolio for industrial identification by adding the Simatic RF200 RFID system with particularly compact readers for the high-frequency range. more
To make it easier for customers to select the right converter for their particular application, the Siemens Drive Technologies Division now provides a means of selecting the appropriate products via the respective application. more
The Siemens Drive Technologies Division will be using this year’s Hanover Fair as a platform to showcase the considerable progress made in its strategic three-pronged integration approach. more
New components with integrated security functions from the Siemens Division Industry Automation allow companies to enhance the safety of their networks in process automation and production automation. more
The Siemens Industry Automation Division has expanded its range of Simatic-S7-300 controllers and improved their performance. In the compact class, all six CPUs have been completely redesigned. more
With the Sinamics G120C, Siemens Drive Technologies Division is extending its product portfolio for this series of inverters. The compact device has been designed for global application in industrial environments. more
The Siemens Drive Technologies Division now offers IEC motors consistently across the efficiency classes IE2 and IE3 covering the application range of EU Regulation 640/2009 from 750 W to 375 kW. more
A new range of Logo! logic modules has been equipped by the Siemens Industry Automation Division with an integral Ethernet interface. more
The Siemens Drive Technologies Division has optimized the design of its 1FK7 servo motor series for standard motion control applications and extended its range of motors in the field of low rated speeds. more
The use of innovative energy-saving technologies not only helps conserve the environment, it also reduces costs and makes for investment security. more
The Siemens Industry Automation Division today introduced the industry’s first automation software with One Engineering Environment and One Software Project for all automation tasks called the Totally Integrated Automation Portal (TIA Portal). more
The Siemens Industry Automation Division has extended its range of Simatic HMI operator panels to include a new series of devices offering high performance and integrated functionality for demanding visualization tasks. more
Drive technology is one of the keys to the sustainable development of future-oriented technologies according to the “Trendts” study commissioned by the Siemens Drive Technologies Division: Drive technology will increase efficiency in production, transport and energy, for instance through the application of self-monitoring field devices or the low-maintenance transport of liquids. more
Combining industrial software with automation engineering opens the door to substantially reduced times to market for new products and a far more speedy return on investment. more
Two new key panels from the Siemens Industry Automation Division feature eight large, programmable keys with backlighting that can be adjusted in terms of brightness and color. more
With Digital Express Design Siemens Industry Automation Division is offering a completely new process for designing customized Simatic HMI unit fronts quickly. more
The new Simatic WinCC V11 HMI software from the Siemens Industry Automation Division is suitable for everything from machine-level applications to process visualization. more
The new Simatic Step 7 V11 engineering system from the Siemens Industry Automation Division is suitable for all controller families, from the Simatic S7-1200 and the Simatic S7-300 and -400 controllers, right up to PC-based automation with Simatic WinAC. more
The Siemens Industry Automation Division has added a new 3" device to its range of Simatic HMI Basic Panels for operating tasks in the lower performance range. Simatic KP300 Basic mono PN has a monochrome display with a high resolution of 240 x 80 pixels. more
The 1PH8 range of motors for main drives developed by the Drive Technologies Division of Siemens has now been extended by models equipped with specially energy-efficient Electronically Commutated (EC) force ventilated fans. more
The Siemens Drive Technologies Division is supplementing its energy-efficient IEC low-voltage motors with two new frame sizes for the aluminum range and is also increasing the power rating on the rugged cast iron range of motors. more
The Siemens Industry Automation Division has added new Profibus, Profinet and telecommunication services to the communication functions of the Simatic S7-1200 controllers. New CPU firmware enables communication with Profinet IO devices. more
There are new additions to the Sitop Smart and Sitop Compact power supply families from the Siemens Industry Automation Division. more
With new products, the Siemens Industry Automation Division is strengthening its RFID (Radio Frequency Identification) product portfolio in the UHF (Ultra High Frequency) frequency range. more
The Siemens Industry Automation Division is expanding its TeleService (remote maintenance/diagnostics) and Telecontrol ranges with three new products for remote access by mobile radio. more
The Siemens Industry Automation Division has developed new network management software that continuously monitors and visualizes the topology, availability and performance of industrial Ethernet networks. more
The Siemens Industry Automation Division has added the Sirius M200D motor starter to its Profienergy-compatible products. The device type was therefore expanded with Profienergy functionality. more
The Sizer software from Siemens Drive Technologies Division is an engineering tool for planning drive applications with Sinamics. more
Siemens´ Industry Automation Division has added new functions to its Logo!Power range of miniature power supply units. more
Siemens Industry Automation Division has added Foundation Fieldbus certified communications to the Sitrans LR250 radar level transmitter. more
The new heavy-duty motion-sensing switch Sitrans WM100 of Siemens Industry Automation Division is used to detect the absence or presence of motion on rotating, reciprocating, or conveying equipment. more
Siemens is extending its range of solar inverters for commercial photovoltaic plants for the power range up to 500 kilowatts. A thin-film photovoltaic plant with an output of 500 kilowatts covers the equivalent area of about three football fields. more
The new Sinvert PVS device line for medium-sized and large photovoltaic power plants supplements the range of solar inverters offered by the Siemens Industry Automation Division. more
The Siemens Industry Automation Division has expanded its Sitop smart series of power supplies with a 24V unit with 3-phase connection. The Sitop PSU300S is designed for standard regulated 24V direct voltage requirements for machinery and plants. more
The Siemens Industry Automation Division has expanded its portfolio of mid-range and high-range S7-300 and S7-400 Simatic controllers and improved their performance. more
Siemens Industry Automation Division has developed a new ultrasonic flowmeter for the hydrocarbon industry, the Sitrans FUT1010. more
From June 16, 2011 machine builders are only permitted to use high-efficiency motors with a minimum efficiency class of IE2. The new EU Directive 2005/32/EC is applicable to low-voltage asynchronous motors of 0.75 to 375 kW. more
With the Sinamics BOP-2 (Basic Operator Panel) the Siemens Drive Technologies Division has brought a new version of its operator panel on the market. more
At this year’s Hanover Fair, Siemens is setting out to answer some of industry’s most pressing questions with an integral array of automation solutions for industrial processes: “The combination of industrial software with automation technology provides the key to a considerably shorter time-to-market of new products and a clearly faster Return on Invest”, explained Anton Huber, CEO of the Industry Automation Division, at Tuesday’s press conference in the run-up to the Hanover Fair. more
The Siemens Drive Technologies Division has now also integrated the "Safely Limited Speed" (SLS) safety function into its Sinamics S110 and S120 motion control converters without using an encoder. more
New 12V and 24V power supplies for the lower performance ranges up to 30W have been developed by the Siemens Industry Automation Division. more
The Siemens Industry Automation Division has now improved the performance of the two technology modules 2 PULSE and 1 STEP for the Simatic ET 200S distributed I/O system and has also added new functions. more
The Siemens Industry Automation Division has brought onto the market a simple lock-and-release plug-in connector for space-saving LC (local connector) connection of fiber-optic cables. more
The Siemens Division Industry Automation has fitted three of their Industrial Ethernet switches with PoE (Power over Ethernet) functionality in accordance with IEEE 802.3af. more
The Siemens Industry Automation Division has added two metal enclosure versions to its range of 3SE5 Sirius position switches. Designed with a high IP66/67 degree of protection, they are particularly suitable for operation in harsh industrial environments. more
With two new signal modules for simple temperature measurement and control applications, Siemens Industry Automation Division has expanded its Simatic S7-1200 compact controller family. more
The Siemens Industry Automation Division has added new functions to the Step 7 Basic engineering system for the Simatic S7-1200 controller and the Simatic HMI Basic Panels. more
The new remote data manager Sitrans RD500 in one device integrates web access, alarm event handling and data capture for remote installed process instruments. more
The Siemens Industry Automation Division has developed four new Simatic S7-300 controllers with a width of just 40 millimeters: the standard controllers CPU 315-2 PN/DP and CPU 317-2 PN/DP and the failsafe controllers CPU 315F-2 PN/DP and CPU 317F-2 PN/DP. more
The Siemens Industry Automation Division has innovated its Sirius Modular System up to 40 A in the main circuit and control circuit. more
The Siemens Industry Automation (IA) and Drive Technologies (DT) Division presentation at this year’s SPS/IPC/Drives in Nuremberg focuses on enhanced efficiency through comprehensive energy management, integrated engineering tools and innovative automation concepts. more
At the SPS/IPC/Drives Fair in Nuremberg the Siemens Drive Technologies Division will be presenting its new modular frequency inverter SINAMICS G120P which has been specially designed for pump, fan, and compressor applications. more
Industry Automation, a Siemens division, has developed a new generation of its sonar proximity switches Simatic PXS. The new sensors of the compact series in M30 design have a reduced blind zone and are shorter than models of the previous generation. more
A new adapter from the Siemens Industry Automation Division makes it easy to integrate standard sensors into the IO-Link, the communication standard for the sensor/actuator level. more
The Sentron PAC3100 Power Monitoring Device from the Siemens Division Industry Automation records energy consumption and measures basic electrical values such as current, voltage, power, and frequency in low-voltage power distribution. more
The range of Industrial Ethernet switches from the Siemens Industry Automation Division has been expanded. more
Siemens Drive Technologies is supplementing its Sinamics G120 frequency inverter series with a new Control Unit specially designed for pumps, fans and compressors. more
The Siemens Industry Automation Division has developed two new communications processors for connecting PCs and S7-300 controllers to Profibus and Industrial Ethernet, respectively. more
The new electronic Sitop PSE200U selectivity module from Siemens Industry Automation Division monitors up to four 24 volt load feeders for overloads and short circuits. more
Siemens´s Industry Automation Division has extended its range of Sirius 3RA6 compact starters to include a model with IO-Link. Several compact starters can be mounted side-by-side. more
The new Simatic S7-1200 Micro-Controller from the Siemens Industry Automation division is characterized by its versatile and flexible setup concept, along with high performance and an extremely compact design. more
The IO-Link sensor portfolio of the Siemens Industry Automation division now includes a product family of ultrasonic proximity switches. more
The Siemens Industry Automation Division is supplementing its portfolio of distributed motor starters with a version that features a higher degree of protection for spatially distributed drive applications. more
Siemens Drive Technologies has expanded its range of drives to include a decentralized frequency converter with degree of protection IP 65. more
Siemens´s Industry Automation Division has produced a new inductive proximity switch for the precise analog and dynamic measurement of distances from metal objects. more
The new Sentron PAC4200 power monitoring device from the Siemens Industry Automation Division collects and records measured data such as voltage, current and energy consumption and permits the analysis of network quality. more
The Siemens Industry Automation Division is complementing its Simatic HMI (Human Machine Interface) device series with all-round IP65 protection with modular expansion units. more
The Siemens Industry Automation Division has developed new Logo! basic devices. The logic modules of the 0BA6 series are significantly more powerful than their predecessor models. With 200 function blocks, the memory capacity is fifty percent larger than before, and the analog inputs have been doubled to four. more