SIMATIC S7-SCL

Structured Control Language

Description

SIMATIC S7-SCL

S7-SCL is particularly suitable for programming complex algorithms and arithmetic functions or for data processing tasks.. S7-SCL combines language elements known from high-level language programming, such as serial loops, alternative branching and branch distributors with language extensions typical for PLCs, such as addressing of inputs and outputs or start and querying of timers and counters.

S7-SCL corresponds to the textual high-level language ST (Structured Text) defined in the standard IEC 61131-3 and fulfills base level and reusability level requirements acc. to PLCopen.

Additional benefits over LAD, FBD, and STL:

  • Simpler, faster, and less error-prone program development thanks to the use of powerful language constructs such as IF...THEN...ELSE.

  • Easier to read, clearer structuring.

  • Simpler program test using a high-level language and a debugger.


Design and functions

S7-SCL programs are programmed as ASCII sources. An exchange with other ASCII sources or targets is therefore possible. The S7-SCL editor offers various templates that only need to be filled in and inserted:

  • Templates for blocks (e.g. function blocks, data blocks) and their calls

  • Templates for block comments, block parameters and constants

  • Templates for control structures (IF, CASE, FOR, WHILE, REPEAT) that contain the exact syntax.

S7-SCL offers the following functionalities:

  • Language elements from programming in high-level languages, e.g. serial loops, alternative branches and branch distributors

  • S7-SCL-blocks can be used in other STEP 7 languages

  • PLC-typical language extensions, e.g. addressing of inputs and outputs, or start and scanning of timers and counters.


Licensing

  • S7-SCL is part of the > STEP 7 Professional Software package yet also available separately

  • S7-SCL V5.6 is delivered with a floating license which allows you to install the software on as many computers as you like. For each license, one user can use the software no matter what computer they’re on, or where they’re working. The number of licenses determines the number of computers the software can be used on at one time

  • There is an upgrade to version 5.6 for the users of the previous version 5.3

  • You can subscribe to a S7-SCL Software Update Service contract as well

Software/Licenses

Article No.

S7-SCL V5.6

You can find more information about SIMATIC licenses, the Software Update Service, the topic Online Software Delivery and how you get supported by the tools Automation License Manager and SUS Manager at: