SIMATIC S7-GRAPH

Programming sequence controls

Description

SIMATIC S7-GRAPH

SIMATIC S7-GRAPH is based on the STEP 7 programming software. It is used for describing procedures with alternative or parallel step sequences. The procedures are configured and programmed clearly and quickly in a standardized method of representation (to IEC 61131-3, DIN EN 61131).The process is described graphically, and divided into individual steps with an easily comprehensible scope of functions.

Actions can be defined for the steps, and their execution controlled. Transitions control the conditions required for the next step. Interlock and monitoring conditions are defined for each step.

Area of application

A typical example of a sequential operation is a drilling procedure with the following steps:

  • Drilling machine ready

  • Clamp workpiece

  • Start drill motor, optionally coolant pump on

  • Lower drill

  • Raise drill

  • Coolant pump off, motor off

  • Open the clamp

For programming compliant with IEC 61131-3 and PLCopen Base Level, the following functions are available.

Benefits

Additional benefits over LAD, FBD, and STL:

  • LAD, FBD and STL focus on logic control. S7-GRAPH places more importance on the pfrocess sequence.

  • Clear graphical representation of the process using sequencers, providing easy maintenance and modification adaptation of the programs if required.

  • Process error troubleshooting with integrated diagnostics functions; expensive downtimes during production are minimized.


Design and functions

Flexible sequencer structure:

  • Simultaneous and alternative branches,

  • jumps within the sequencers,

  • step enabling and disabling.

Selective processing of steps. The processing time of a sequencer is thus independent of the number of steps.

Synchronizing automatic and manual operation. The process is not synchronous anymore when it was placed into a different state manually.

S7-GRAPH supports the locating of synchronization points for restarting automatic operation. To do so, the relevant steps are marked. Step-enabling conditions or interlocks can be defined as criteria.

Licensing

  • S7-GRAPH is part of the > STEP 7 Professional Software package yet also available separately

  • S7-Graph V5.6 is delivered with a floating license which allows you to install the software on as many computers as you like. For each license, one user can use the software no matter what computer they’re on, or where they’re working. The number of licenses determines the number of computers the software can be used on at one time

  • There is an upgrade to version 5.6 for the users of the previous version 5.3

  • You can subscribe to a S7-GRAPH Software Update Service contract as well

Software/Licenses

Article No.

S7-Graph V5.6

You can find more information about SIMATIC licenses, the Software Update Service, the topic Online Software Delivery and how you get supported by the tools Automation License Manager and SUS Manager at: