Connection of drive components

Description

The technology controllers have an isochronous DP(DRIVE) interface for connecting the drive components. This is optimized for connection of drives over PROFIBUS – all Siemens drives are supported

Connection of the components to the technology CPU via DP(MPI) and PROFIBUS DP(DRIVE)

The PROFIBUS DP (DRIVE) interface supports isochronous mode and therefore provides an essential requirement for controlling high-speed and time-critical operations such as are found in distributed axes in synchronized applications. The interface can only be used as a DP master. It serves to connect drive components. In addition to drive systems, DP-V0 slaves can also be operated on the DP (DRIVE) line on a limited basis.
 

Supported components on

PROFIBUS DP(DRIVE)

Speed-controlled axes

MICROMASTER 420/430/440
COMBIMASTER 411
SIMOVERT MASTERDRIVES VC

Positioning/synchronized axes


SIMODRIVE 611 universal HR
SIMOVERT MASTERDRIVES MC
SIMODRIVE POSMO CD/SI/CA
SINAMICS S120

Other PROFIBUS nodes


SIMODRIVE sensor isochronous
ADi 4 analogedrive interface module
IM 174
ET 200M with IM 153-2 High Feature
ET 200S with IM 151-1 High Feature


06/24/2010 | Author: Name