The Siemens Industry Automation Division is expanding the Sitop power supply portfolio with the PSU100D switched-mode power supply systems. The new products are single-phase devices with an attractive price/performance ratio for direct mounting on a wall. more
The Siemens Industry Automation Division has expanded its power supply offering with the new product range Sitop lite. more
Siemens Industry Automation Division is launching a rugged power supply unit onto the market with a high degree of efficiency of 96 percent. more
There are new additions to the Sitop Smart and Sitop Compact power supply families from the Siemens Industry Automation Division. more
Siemens´ Industry Automation Division has added new functions to its Logo!Power range of miniature power supply units. more
The Siemens Industry Automation Division has expanded its Sitop smart series of power supplies with a 24V unit with 3-phase connection. The Sitop PSU300S is designed for standard regulated 24V direct voltage requirements for machinery and plants. more
New 12V and 24V power supplies for the lower performance ranges up to 30W have been developed by the Siemens Industry Automation Division. more
With a width of only 90mm, the new Sitop PSU100M DIN rail power supply unit from the Siemens Industry Automation Division is 40 percent narrower than its predecessor. more
The new electronic Sitop PSE200U selectivity module from Siemens Industry Automation Division monitors up to four 24 volt load feeders for overloads and short circuits. more
Siemens´s Industry Automation Division has developed two new 3-phase, 24 volt power supplies: the Sitop PSU300P and the Simatic ET200pro PS. more
Siemens Industry Automation Division has equipped its new uninterruptible 24 volt Sitop UPS500S power supply for direct voltage systems with an innovative, maintenance-free capacitor system. more
Siemens Automation and Drives (A&D) is supplementing its Sitop power supplies with a new range of stabilized units for the low-end performance range. more