SINUMERIK 840D sl - Watch videos

Additive Manufacturing and Machining - The integrated Siemens process chain in practice

The Hoedtke GmbH & Co. KG company is one of the first manufacturing companies using an industry-standard DED overall solution: From the CAD/CAE/CAM process with the Software Suite NX through to the printing and machining processes performed on a high-performance machine equipped with SINUMERIK 840D sl.


Research and innovation with SINUMERIK

SINUMERIK - a success model: In his research activities, the WZL Aachen relies on a Mazak Variaxis i-600 5-axis machining center with SINUMERIK 840D sl CNC. The complete system including dynamic machine building and innovative CNC technology optimally meets the requirements arising in gear wheel manufacturing: Repeat accuracy together with superior surface quality.


Smart Operation with SINUMERIK

With Smart Operation, SINUMERIK opens the door to new concepts in machine operation. Here, on the one hand, our new panel generation is important: the SINUMERIK blackline panel with touch and gesture operation. On the other hand, SINUMERIK supports the use of terminal devices in manufacturing.


Multitasking with SINUMERIK 840D sl at Mazak

In its multi-functional machines, Mazak now also goes for Siemens technology. The comprehensive CNC-functions in SINUMERIK and the consistent look and feel in operation and programming with SINUMERIK Operate allow maximum CNC performance and user friendliness in multitasking applications.


SINUMERIK Collision Avoidance at Gebr. Heller

In the new multitasking machine series CF, Heller goes for realtime collision avoidance in SINUMERIK. With Collision Avoidance SINUMERIK offers the best possible protection from unintentional collisions in the machining space of the machine tool -- specifically, between moving and static machine components. This is an important means of protection whenever the operator intervenes in the process.


Multitasking with CNC SINUMERIK 840D sl

Concerning machine tools, there is a trend towards multitasking machines: turn-milling oder mill-turning machines. Here, the strength of the CNC control SINUMERIK 840D sl and SINUMERIK Operate becomes evident. With that, all users can conveniently operate a multitasking machine.


SINUMERIK 840D sl and XL segment motor at ELHA

The complete machining centers from ELHA are equipped with SINUMERIK 840D sl. Further, the Siemens Mechatronic Support has developed a customized segment motor with 18 stator segments, a maximum speed of 100 rev/min and a diameter of 3.42 m for ELHA. The ELHA customers benefit from utmost machining accuracy in XL format.