Flyer

The flyer is located in the spinning process between the drawing frame and the ring spinning frame. It produces a suitable roving for the ring spinning frame. The already drawn fiber tape is further drawn out in the flyer. Major components of the flyer are the feeding gate, the drawing equipment and the flyer frame.

Usually 4 motors are required on the converter. An asynchronous motor with about 11 kW is used for the drawing equipment, while one servo motor each is used for the lifting motion, the flyer wings and the spindles (MO approx. 18-36 Nm).

Benefits

High productivity

  • through multi-axis control

  • through minimum setup times

  • through electronic gear factor presets